Issue
TGML Objects are not highlighted when dragging and dropping snippets to the graphics editing pane. If a number of objects are close together, it can be difficult to see which object the snippet is being dropped on to.
Product Line
TAC Vista
Environment
TAC Vista 5.1.7
TGML editor 5.1.7
Cause
Updates to the TGML Editor in 5.1.7 removed this feature.
Resolution
The item which the mouse-pointer is hovering over is highlighted in the TGML menu tree in later versions. An upgrade will restore this functionality.
As a workaround in version 5.1.7, snippets can be dragged directly to the desired object in the Objects Pane as opposed to the editor workspace to ensure the proper object is selected.