Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Suprema Fingerprint Reader Integration

Issue

Suprema Fingerprint Reader Integration

Product Line

Security Expert

Environment

  • Security Expert
  • Suprema Fingerprint Reader

Cause

Security Expert integrates with Suprema BioEntry, BioEntry Plus, and FaceStation devices. Enrolment is both quick and easy. Users scan their fingerprint or face at an enrolment reader. The reader uses the scanned data to create a credential template, including a card number, which it sends to the Security Expert Server. Security Expert then sends this template to any other Suprema readers that are attached to the system, so the user only needs to enroll once.

Resolution

The following information is available on integrating Suprema Fingerprint Readers with Security Expert

  1. A list of qualified Suprema devices and configuration details can be found in the Suprema Biometric Integration in Security Expert Application Note.
  2. There are some available help topics in the online help. In the Security Expert  Client go to ABOUT | HELP and search for "Biometric Readers" and "Suprema".
  3. Each Suprema reader requires a wiegand port on a controller / expander, a license (SX-BIO-SP) and an IP address. The amount of Suprema readers allowed is only limited by these numbers. 
Tags (1)
Labels (1)
No ratings