Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Supported communications options when running VisiSat software on Windows 7

Issue

Update to available documentation.

Product Line

EcoStruxure Building Operation, Satchwell MicroNet

Environment

Windows 7 32/64 bit

Cause

Clarification of supported communication protocols and devices.

Resolution

Computer running Windows 7 32bit or 64bit.
Visio software installed must be 32 bit version.
VisiSat runs as a 32 bit application.

SNP
Via computers RS232 communications port.
Via RS232 provided by USB to RS232 converter.
Via RS232 provided by PCMCIA card to RS232 converter.
Via RS232 provided by Express card to RS232 converter.
IP tunneling through Xenta 555/731 AS/AS-P LAN network.
Remote site connection.

NCP
Via computers RS232 communications port.
Via RS232 provided by USB to RS232 converter.
Via RS232 provided by PCMCIA card to RS232 converter.
Via RS232 provided by Express card to RS232 converter.
IP tunneling through LAN network.
Remote site connection.

ARCnet
Via computers RS232 communications port connected through null modem lead to an MicroNet Interface Unit. (MN50-MI-ARC).
Via PCI120U-485 PCI card  (This card was made by Contemporary controls but is no longer). The card was replaced by the USB22 Series. (USB 2.0 to ARCNET adapters) These USB22 adapters do not work with VisiSat.
IP tunneling through LAN network.
Remote site connection.

LON
Not supported with Windows 7 64bit or 32bit. 

The latest documentation for VisiSat can be downloaded, see Download latest VisiSat Data Sheets, Engineering Guides, Installation and User Guides, and Release N....

Tags (1)
No ratings