New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements

- Who are the top users of September? Discover them here!

- Check out the ESS Active Energy Management Blog now! 

- Join us on October 23rd for a live Panel session to discuss The Power of a Sustainable Ecosystem with Hervé Coureil, Chief Digital Officer of Schneider Electric and other great speakers. Register here!

Supported camera conditions to be shown as a Continuum alarm

Issue

What camera conditions does Continuum support being shown as a Continuum alarm?

Product Line

Andover Continuum, Pelco

Environment

  • Continuum v2.0
  • Pelco Video Server
  • Digital Sentry
  • Endura

Cause

Available documentation is a bit bare on specifically what camera conditions can be monitored / setup to be displayed as alarms in Continuum.

Resolution

According to the latest Video Compatibility Matrix, only the following video alarms are supported:

  1. Video server online/offline
  2. Camera video loss (cable connection loss only, not covering of camera lens)
  3. Motion detection (per camera)

Note: Video loss and motion alarm functionality are not supported on DVX and DVXi Video Servers.

Tags (1)
Labels (2)
No ratings