New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

StruxureWare Building Operation supported MicroNet devices

Issue

StruxureWare Building Operation Satchwell MicroNet Integration - Supported MicroNet devices

Product Line

EcoStruxure Building Operation, Satchwell MicroNet

Environment

  • StruxureWare Building Operation 1.3, 1.4, 1.5, 1.6
    Satchwell MicroNet devices

Cause

Not all variants of older Satchwell MicroNet devices that use the SNP protocol and IAC are supported by StruxureWare Building Operation. 

Resolution

Refer to MicroNet Devices on StruxureWare Building Operation Web Help (log on required) for a list of supported devices. 

In Building Operation, MicroNet device is the family name for the following devices:

  • Standard MicroNet devices: MN300, MN440, MN500, MN620, MN LCD, MN Touch Screen, and MicroNet Manager Interface
  • MN 50 Series: MN350, MN450, MN550, MN650, MN LCD, MN Touch Screen, and MicroNet Manager Interface
  • SNP and Intelligent Advanced Controller devices: MMC3601, MMC4601, IAC400, IAC420, IAC600, IAC Touch Screen, and Modem Interface Unit
  • Unifact: URC2201, URC1201
  • Unifact Pro: URC-40N-100, URC-41N-10x, URC-50N-100, and URC-51N-10x

All these devices are supported in Building Operation.

Tags (5)
No ratings