Issue
Sigma 4.05 SP1 client does not seat after new install
Environment
Sigma 4.05 SP1
Cause
When you install Sigma 4.05 SP1 on a computer that does not have a the Sentinel Protection driver previously installed, the Sentinel Protection software is not installed.
Resolution
When you install Sigma 4.05 SP1 on a computer that does not have a the Sentinel Protection driver previously installed, the Sentinel Protection software is not installed. This driver has to be installed for Sigma to run.