Issue
Serial Commport Settings when using Roam IO/2
Environment
RoamIO/2
Cause
Serial commport settings
Resolution
The serial commport settings used to connect to the Roam IO/2 tool are listed below.
Bits per second: 9600
Data bits: 8
Parity: None
Stop bits: 1
Flow control: None
When using the Roam IO/2 with a Serial Cable, please make sure cable uses the following pinout assignments.
Pin Signal 2 RXD (Received Data)
3 TXD (Transmitted Data)
5 GND (Ground)
NOTE: In the field we've seen some success when using USB to Serial converters, but not all devices will work. Using Serial 9 pin to 9 pin with the above configurations is the preferred method for Serial connection.