Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Security Expert supported fingerprint readers

Issue

What Fingerprint readers does Security Expert support?

Product Line

Security Expert

Environment

  • Security Expert
  • Fingerprint Reader

Cause

Require information on what Fingerprint Biometrics are supported with Security Expert.

Resolution

We only officially support Suprema Biometric readers (HLI p/n SX-BIO-SP) however our reader expanders/controllers should be able to be connected/work with any reader that outputs a standard 26-bit Wiegand output.

If there is a fingerprint reader that does this it should be able to be connected to Security Expert like a standard card reader supplying the controller with Wiegand data that is assigned to a user's fingerprint. The enrolling of fingerprints etc would need to be handled by the third party system, we would essentially be treating it as a normal card reader and card.

The integration with Suprema Biometric readers allows you to enroll the users fingerprints to the biometric device from within the Security Expert UI.

For a list of Suprema devices that Security Expert supports refer to the Suprema Biometric Integration in Security Expert Application Note.

Tags (1)
Labels (1)
100% helpful (1/1)