Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Replacing Satchwell Sensors with Schneider Electric part numbers

Issue

Replacing Satchwell Sensors with Schneider Electric part numbers

Product Line

Field Devices

Environment

Sensors

Cause

Cross referencing older 'T' type sensors to the current version.

Resolution

  • Outside Sensor DOT2301 , DOT0001, DOT0002 is now STO600
  • Immersion Pipe Sensor DWT1701 (125mm), DWT1702 (200mm), DWT0001 is now STP660 (note, if replacing sensor only then DWA0001 required).
  • Strap On/Pipe Contact Sensor DST1601 , DST0001 is now STC600
  • Duct Sensor (mainly FCUs) DDU1803 , DDU0001 is now STD670
  • Duct Sensor DDT1701 (300mm) , DDT1702 (460mm) , DDT0001 is now STD660
  • Room Sensor DRT3453 (sensor only, no setpoint adjust) is now STR600
  • For other DR and DRT sensors see Replacements for Satchwell sensors
  • Drayton Room Sensor A701 is now STR600D
  • Drayton Outside Sensor A702 is now STO600D
  • Drayton Immersion Sensor A703 is now STP600D
  • Drayton Strap On / Contact Sensor A704 is now STC600D
Tags (4)
Labels (1)
No ratings