Issue
Replacement controller for the KMC 3201.
Product Line
Field Devices
Environment
- KMC
- 3201
- application 4
Cause
The KMC 3201 is no longer available.
Resolution
The KMC 3201 is a multi-application configurable controller, and this article only deals with replacing a controller running application 4, Two stage temperature control.
For the KMC data sheet please click HERE.
The replacement for the KMC 2301 using application 4, is the CZT5305, click HERE for the data sheet.
Please note this is not a like for like change, installation and wiring changes will be necessary.