New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Replace 7792 (7790) and 7793 (7790A) LIU with 7798C

Issue

Separate a 7792 or 7793 into two 7798C

Product Line

TAC INET

Environment

  • Site using I/NET

Cause

Need to replace a 7792 or 7793 which is two channels (A&B) and replace with two 7798C

Resolution

Make a backup of the I/NET Seven system using DBCreate.

Then making sure that your SAV files are current for the 7792 or 7793, send those as attachments to Product Support. We can separate and send back two separate SAV files. Those files will need to be renamed to the appropriate name for the new 7798C.

 

Example:
one 7793 split into two DCUsave files:
Original DCU0101.SAV becomes
DCU0101.sav = Old 7793 “A” channel
DCU0102.sav = Old 7793 “B” channel
 

For SAV file upgrade information see How to upgrade bin and SAV files in I/NET controllers.

Tags (4)
Labels (1)
No ratings