Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Repair options for an MSC-LIM

Issue

To communicate directly with a laptop to a DMS Microsmart controller requires an interface adapter. The model number of the adapter is MSC-LIM. It is obsolete. Does it have a replacement?

Product Line

TAC IA Series

Environment

  • DMS
  • Microsmart revision 10 and 11

Cause

Obsolete part

Resolution

There is no replacement for the MSC-LIM, but there is a repair option.

See Repair or replace an obsolete part from the Network 8000 and DMS product lines.

Tags (1)
Labels (1)
No ratings