Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Redundancy TVDA

Issue

How to be redundant with your intelligent Building Management System (iBMS)

Environment

  • Existing intelligent Building Management System
  • Open Mind High Avalibility Solutions
  • everRun MX

Cause

In engineering, redundancy is the duplication of critical components of a system with the intention of increasing reliability of the system. To be redundant with an intelligent Building Management System (iBMS) would take on two possibilities.

1. Have an alarm on critical points alerting personnel who move into action quickly replacing control boards or devices in the event of failure.

2. Have secondary backup controllers which upon failure, which are used to control devices resuming functionality. This is accomplished through programming the BAS with event sequences triggered from alarms or flags noting the failure.

Redundancy capabilities and feasibility is site specific. Ascertaining failure in boards, points, or devices is crucial to creating secondary measure to keep seamless processes going and resume with functions.


 

Error detection and correction with maintenance is often the best practice for preventing failure. Worn components is the leading cause of failure, followed by lack of planning and consideration in the protection of electrical components through power surges or failures.  

For the database, backups including automated backups for MSDE, SQL Express, and Full SQL are available. For further information on database backups and options, take a look at Microsoft SQL Management Studio.

For Host Computer backups, look at adding a secondary computer which replicates the database and can capture transactions and messages should a failure with the primary host computer take place. Also work with the local IT department to keep machines up to date, safe, and clean of 3rd party applications which may interfere with integrity.


 

Schneider Electric’s building management systems are designed such that building control continues even when controller to server communication is disrupted. The BMS server is home to a database of alarm and historical data, as well as system parameters and programs. When a server or its network connection fails, the collection of data from building controllers halts until the problem is resolved. For data critical applications, this solution provides an environment capable of preventing the data loss that results from these types of failures.


 Although we do support its use with StruxureWare Building Operation, Security Expert, Continuum, I/NET, Vista, Sigma, and I/A Series as a disaster recovery solution, we do not provide direct support for EverRun.

Resolution

For Open Mind High Avalibility Solutions guide please look at the following link; Open Mind High Avalibility Solution guide

For everRun MX solution guide please look at the following link; everRun MX guide
 

No ratings
Contributors