Issue
After reviewing a DMS installation, the red end-of-line (EOL) termination modules are not installed on the Microsmart trunk. The original part number was N406-032. Are they available for purchase?
Product Line
TAC IA Series
Environment
DMS
Cause
Part number cross reference
Resolution
The part number is changed to RBSC-16. Use this number when contacting customer support services.