Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Recovery of XBuilder project if no copy is saved and backup was not sent to target

Issue

If there is no saved copy of an XBuilder project and the backup was not sent to target it may still be possible to recover some of the data to be able to reconstruct the project

Product Line

TAC INET, TAC Vista

Environment

Xenta 5xx / 7xx / 9xx

Cause

Lost XBuilder project and backup was not sent to target

Resolution

With XBuilder 1.5.0 or later connect to the Xenta controller through the web interface and use the Utilities > Project Tree to view the project information. Use this information as a blueprint to rebuild the XBuilder project.

If an older version of XBuilder was used then can connect to the Xenta Server with FTP. The OGC graphic files as well as the CFG files which configure the linking of points and signals can be obtained through the FTP. These files can then be imported into a new XBuilder project which can be sent to the Xenta Server.

Tags (1)
Labels (2)
No ratings