Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Procedure to activate the Add-on reports module.

Issue

Procedure to activate the Add-on reports module.

Environment

Continuum Add-on reports module.

Cause

Received an Activation Code from the COE Team, need to know the procedure to activate the Add-on reports module.

Resolution

You will receive an Email from the COE Team with the Activation Code along with Instructions on how to activate it. For your Convenience the instructions are below.

ACTIVATION INSTRUCTIONS - CONTINUUM REPORTS INSTALLED IN C:\PROGRAM FILES

  1. Make sure Continuum is not running
  2. Make sure Continuum Reports is not running
  3. Launch a DOS Command Window
  4. CD "Program Files\Continuum_Reports"
  5. Enter in lower case: reports key writer
  6. Enter the activation code. (Note: Case sensitive)
 
-(OR)-
 

ACTIVATION INSTRUCTIONS - CONTINUUM REPORTS INSTALLED IN C:\PROGRAM FILES (X86)

  1. Make sure Continuum is not running
  2. Make sure Continuum Reports is not running
  3. Launch a DOS Command Window
  4. CD "Program Files (x86)\Continuum_Reports"
  5. Enter in lower case: reports key writer c:\progra~2\continuum_reports
6. Enter the activation code. (Note: Case sensitive)Activation Instructions - Continuum Reports installed in C:\Program Files
1. Make sure Continuum is not running
2. Make sure Continuum Reports is not running
3. Launch a DOS Command Window
4. CD "Program Files\Continuum_Reports"
5. Enter in lower case: reports key writer
6. Enter the activation code. (Note: Case sensitive)
-or-
Activation Instructions - Continuum Reports installed in C:\Program Files (x86)
1. Make sure Continuum is not running
2. Make sure Continuum Reports is not running
3. Launch a DOS Command Window
4. CD "Program Files (x86)\Continuum_Reports"
5. Enter in lower case: reports key writer c:\progra~2\continuum_reports
6. Enter the activation code. (Note: Case sensitive)
Labels (1)
No ratings