New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Announcements

- Discover the Exchange Community Top members of October here!

- Check out the ESS Active Energy Management Blog now! 

- Watch now the replay of The Power of a Sustainable Ecosystem panel with Hervé Coureil and other experts 

Potentiometer input on a Xenta programmable device

Issue

Setting up a potentiometer or resistance input on a Xenta Programmable controller.

Product Line

TAC Vista

Environment

  • TAC Menta
  • Xenta 280,300 and 400

Cause

No input option is available for a potentiometer or resistance in a Xenta device

Resolution

A curve module can be used to create your own input lookup table, as shown below.

Lookup table.png

Attached file Pot_To_0_100_R01.zip provides an example of this 10K potentiometer sample

Tags (2)
Labels (1)
Attachments
No ratings