Issue
Different Windows Users see the Pinpoint buttons differently.
Product Line
Andover Continuum
Environment
Cyberstation Pinpoint
Cause
Continuum uses the information from the Windows profiles to define the system appearance.
Resolution
In the Windows Display properties you can select the "Windows and Buttons" style for your profile, this will change the appearance of the standard buttons used within Pinpoint graphics.
For example:
Selecting Windows XP Style will look like:
Selecting Windows Classic Style will look like:
Windows 7 also has other styles available.