Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Periodical reports is not working in TAC Vista

Issue

  • A report is set up to be printed automatically at certain times using Periodical reports.  

    Nothing happens and the report is never printed.

  • It is possible to open a report manually and print it but the reports are not printed when using periodical reports.

Product Line

TAC Vista

Environment

  • Vista Server
  • Windows Server 2008

Cause

  • The periodical report worked when running Vista as a application but not as a service.
  • The user starting the service Tacos had a password with only three characters which does not meet the complexity requirements for a Windows 2008 server.
  • It was possible to login and start the service using this password but the service Tacos could not start Excel and create the report using this password.

Resolution

Change to a user with a password meeting the complexity requirements for a Windows 2008 server for the service called Tacos.

Tags (2)
Labels (1)
No ratings