Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Part Number for the optional battery for the JACE-NXT (TRD-NXT-R2)

Issue

What is the Part Number for the optional battery for the JACE-NXT (TRD-NXT-R2)?

Product Line

TAC IA Series

Environment

  • I/A Series R2
  • JACE-NXT (TRD-NXT-R2)

Cause

An optional battery is required for the JACE-NXT (TRD-NXT-R2).

Resolution

The part number for the optional battery is TRD-NPB-BATT, per the Spec Data sheet for the JACE-NXT, F-27769.

There is also an optional UPS that includes a battery, TRD-NXT-UPS, per Hardware platforms to replace the I/A Series R2 UNC-600 or UNC-610.

See Product Announcement PA-00223 for further information on the JACE-NXT.

 

*Update - The NXT platform has been withdrawn. Refer to PA-00373 for details. 

Tags (1)
Labels (1)
No ratings