New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements

- Who are the top users of September? Discover them here!

- Check out the ESS Active Energy Management Blog now! 

PIN locations for control for MPT24DT

Issue

What are the PIN locations for right and left control?

Environment

MPT24DT Pan/Tilt functions, PT270-24P, PT280-24P, PT570-24P, PT680-24P

Cause

Loss of manual for PIN layout

Resolution

On either a 14-PIN or a 9-PIN the following applies:                                                                                                                     

  • PIN 1 is P/T common
  • PIN 3 is Left control
  • PIN 5 is Down control
  • PIN 6 is Up control
  • PIN 7 is Right control
  • PIN 8 is Safety Ground

                                                                                  

 

 

  NOTE: MPT24DT can also be used to control 120 VAC pan/tilt  and scanners when used with RB115 relay box                                                                               

Tags (1)
Labels (2)
No ratings