Issue
No stencils in VisiSat software for the new MicroNet 50 series range
Environment
- MicroNet 50 series range
- VisiSat
Cause
An upgrade is required to receive these stencils.
Resolution
- Go to the help menu, and select about VisiSat.
- If you are running VisiSat 2.0 then you need to request the latest version of VisiSat 2.1. VisiSat 2.0 to VisiSat 2.1 is a free upgrade
- If you are using VisiSat 1.1 or VisiSat 1.2, then you will need to purchase VisiSat 2.1.