Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

.NET Framework errors in general

Issue

When launching a program or when working with a program, you get an error from "Microsoft .NET Framework".

Environment

Windows

.NET Framework

Cause

Microsoft .NET Framework is used in almost all larger applications, and there can be various reasons why you see an error. One reason can of cause be application specific, meaning that there is an actual issue with the software and the way the software is using .NET Framework, but another reason can be that the .NET Framework installation itself is corrupted.

If it's an application specific issue, you need to contact product support, but in many cases simply repairing the .NET Framework installation has proven to solve the issue.

Resolution

1: Close all applications

2: Make sure you have the correct version of .NET Framework installed for the software you use referencing the products data sheet. You can use this tool to check what versions you have. Here is a direct download link.

3: Install versions that might be missing. You can download the various versions from the tool linked above.

4: Download Microsoft's .NET Framework repair tool and run it applying all fixes the tool suggests. Here is a direct download link.

Tags (6)
No ratings