New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

NCP network with two or more MicroNet Touchscreens, values in controllers on a sublan are changing unrepentantly.

Issue

On a NCP network where there are two or more MicroNet Touchscreens on the system, some values in MicroNet controllers on the Sub-LAN of a MicroNet Touchscreen are found to be changing unrepentantly.

Product Line

Satchwell Micronet

Environment

Communications

Cause

Micronet Touchscreen error

Resolution

Updated June 2019

The MicroNet 50 series range MN350, 450, 550, 650 LCD and Touchscreen have been withdrawn from sale.
The IAC 420, 600 and Touchscreen have now also been withdrawn from sale.
No direct replacement is offered.
Further information on these changes can be found in PA-00495 - Notice of Withdrawal - Satchwell Sigma and PA-00528 - End of Commercialization - Satchwell Sigma.

----------------------------------------------------------------------------------------------------------------------------------------------------------

The problem generally occurs when there is heavy communication traffic through the Touchscreens.


New Touchscreen firmware version MNTS0H has been released fixing this issue.


The firmware has been tested with VisiSat 2.1 Build 148 Service pack 1, MN50 series controllers, Xenta 555 and Xenta 731 hardware.

Please refer to TPA-LOND-09-0029.00 Touchscreen TS0H firmware.

Tags (2)
Labels (1)
No ratings