Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple custom card formats in Security Expert

Issue

Is it possible to setup more than one custom card format in Security Expert?

Product Line

Security Expert

Environment

  • Security Expert
  • Custom Card Formats

Cause

Have a requirement for two or more custom card formats.

Resolution

Currently, you cannot setup two custom formats.
 
It is possible to add a Secondary Format to a Reader port in Reader-Expanders, but you can only setup one as a Custom Format. They are actively working on adding multiple Custom Formats. There is no ETA on when this will be available.
Tags (1)
Labels (1)
No ratings