Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Minimum display is 1024x768 which is too small for proper screen size

Issue

Minimum display is 1024x768 which is too small for proper screen size

Environment

SmartStruxure up to release 1.3

Cause

Release notes for 1.3 in 9.2.1 state the Minimum display is 1024x768 which is too small for proper screen size.
In the screen capture below, a simple schedule is created, and then a New Schedule Event is selected which opens the window. the window is larger than the screen size, missing the top and bottom.

Resolution

Adjust the screen resolution to a larger size which is suitable. Size is dependent on hardware specifications.

Tags (4)
Labels (1)
No ratings