Issue
.xif file not available for download.
Product Line
Field Devices, Other, TAC Vista
Environment
- MF20-24M 1M54 00
- MF20-24L actuator
Cause
When configuring the MF20-24L in LonWorks, .xif file is necessary.
Resolution
All necessary files for LON connectivity are available here: lon_actuator_v3.0 (1).zip