Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

LinePrinterRecipient 'Load Printer List' does not bring up a list of the available printers

Issue

LinePrinterRecipient 'Load Printer List' does not bring up a list of the available printers

Environment

I/A Series G3 Enterprise Network Server (ENS) or Enterprise Network Controller (ENC).

Cause

At this stage the reason that this occurs is unknown but the following resolution is the current workaround.

Resolution

Since you are not able to find the printer using the 'Load Printer List' button, you should just type in the name of the printer in the LinePrinter Recipient's properties 'Printer' field.

To make sure you get the name correct, go to Windows Control Panel and go to 'Printers and Faxes'. Find the line printer and right-click on it to the properties. Copy the name of the printer. Go to Workbench and paste the name of the printer in the LinePrinter Recipient as per described above.
 

Tags (1)
Labels (1)
No ratings