New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Large change in Database IDs

Issue

There are large jumps in Database ID numbers in the lists of objects in Security Expert. Most notably seen in the Trouble Inputs table.

In the below example the Database ID's in the Trouble Input table jumped from 420 to 1424.

SX_ToubleInput_DatabaseIDs_LargeJumpInID.pngFigure 1 - Database ID's

Product Line

Security Expert

Environment

  • Security Expert Server
  • Security Expert Client

Cause

This is a rare occurrence but when seen can be due to the creation and deletion of Controllers and Expanders as a site is being configured or just normal operation as SQL maintains the Security Expert database.

Resolution

No action required. This is a benign condition which does not affect the normal operation of Security Expert.

Tags (1)
Labels (1)
No ratings