Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

It is not possible to write to any parameter in the IAC400, IAC600, MMC3601 or MMC4601;

Issue

It is not possible to write to any parameter in the IAC400, IAC600, MMC3601 or MMC4601; reading is not a problem. This is because VisiView is attempting to write an EEPROM value that is not supported by these devices. IAC420's are not affected. VisiSat is able to write parameters to all these devices.

Environment

VisiView

Cause

Global time update is currently being transmitted to Group 1. This has been corrected to transmit as Group 0.

Resolution

Install service pack 3

Click here to download service pack 3

Click here to view the release note for service pack 3

Click here to download the release note for service pack 3

Tags (1)
Labels (1)
No ratings