Issue
Issues with some portions of Vista 5.1 on Microsoft Windows Vista
Environment
- Microsoft Windows Vista
- TAC ToolPack
- TAC Signature
- TAC Webstation
- TAC OPC Server for Danduc
Cause
Not all portions of Vista 5.1 are supported on Microsoft Windows Vista.
Resolution
While TAC Vista supports Windows Vista in release 5.1.0 the following programs are not supported:
- TAC Toolpack
- TAC Signature
- TAC Webstation
- TAC OPC Server for Danduc
Note: This is still true for version 5.1.1 despite this only being stated in the Vista 5.1.0 release notice.