Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Issue capturing personnel photo from USB camera in Create/Edit badge dialog.

Issue

In the 'Make/Edit Badge' dialog of the personnel manager/editor, selecting 'Capture Photo' but nothing happens.

USB camera device works fine from an application other than Continuum.

Environment

CyberStation

Cause

The photo image source has not been properly selected.

Resolution

In the 'Tools' menu select 'Set Photo Image Source' menu item then select the camera device and click OK.

Clicking the 'Capture Photo' button works once the camera has been selected as the source.

Tags (1)
Labels (1)
No ratings