Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Is there an object in I/A Series R2 (Niagara) that can make Enthalpy calculations?

Issue

Is there an object in I/A Series R2 (Niagara) that can make Enthalpy calculations?

Environment

I/A Series R2 (Niagara) station, build (X, to be determined)

Cause

Need enthalpy calculation.

Resolution

Consider the following two program objects:

1. tridiumx / lib/ programObjects / hvac/ Psychrometric Calculations.sns

// Psychrometric Calculations
//
//   This object calculates enthalpy, wetBulb and dewpoint for
//   inputs of dry bulb temperature and relative humidity.
//
//   NOTE: This object REQUIRES the lib.jar file be present.



2. tridiumx / lib/ energyManagement / OutsideAirOptimization.sns

// Outside Air Optimization
//
//   This object uses the two sets of temperature and humidity inputs
//   to find the air supply with the least amount of heat.  The freeCooling
//   output will be set to false if outside >= inside
//   and set to true if outside <= inside - (abs)thresholdSpan.
//   The user can select temperature or enthalpy comparisons.
//   There is also a low temperature check to protect against freezing.
//
// Revision History:

Tags (1)
Labels (1)
No ratings