Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a way to determine which version of Operator Interface is installed without actually running the program?

Issue

Is there a way to determine which version of Operator Interface is installed without actually running the program?

Environment

DMS

Operator Interface

Cause

Determine the version without running the program

Resolution

Open the file LANGUAGE.TXT in the DMS folder using Notepad and line 12 will indicate the version installed:

Tags (1)
Labels (1)
No ratings