Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Is the SE7000 series controllers with LonWorks communications compatible with TP/FT -10 channels?

Issue

Is the SE7000 series controllers with LonWorks communications compatible with TP/FT -10 channels? 

Environment

SE7000 series controllers

Cause

The datasheet indicate network compatibility with Echelon LonTalk but there is no mention of the compatibility with TP/FT-10 channels / networks. This may be unclear to some. 

Resolution

The SE7000 series is compatible with LonWorks TP/FT-10 channels. Refer to the datasheet for 14240R which is the free topology transceiver used in the SE7000

capacitors, LPT-10 Link Power Transceivers
Free Topology Transceivers, and, with suitable DC blocking
capacitors, LPT-10 Link Power Transceivers
FT 3120 / 3150 s mart Transceivers, FTT-10 and/or FTT-10A
Free Topology Transceivers, and, with suitable DC blocking
capacitors, LPT-10 Link Power Transceivers
Tags (4)
No ratings