Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Interchangeability of Different Models of AS-B

Issue

Need to know if various AS-B footprints and their databases are interchangeable. 

Environment

AS-B

AS-B-24

AS-B-24-L

AS-B-24-H

AS-B-36

AS-B-36-L

AS-B-36-H

Cause

There are several different footprints and versions of the AS-B hardware. This can cause confusion on whether these servers are interchangeable. Below are are few example scenarios:

 

  • Can an AS-B-24 be replaced with an AS-B-24-L?

 

  • Can a backup from and AS-B-36-L be restored into an AS-B-24? 

 

  • Can a backup from and AS-B-24-L be restored into an AS-B-36-L?

Resolution

The answer to all of the above scenarios is "No". The various AS-B hardware ARE NOT INTERCHANGEABLE. Backupsets can only be restored from one AS-B to another AS-B of the EXACT SAME HARDWARE TYPE. If an import of one type of AS-B into a AS-B of a different hardware type is attempted, the error below will be encountered. 

 

Tags (5)
Labels (1)
No ratings