Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Installing Webclient over the top of Cyberstation

Issue

At times a webclient install is needed but a Cyberstation installation was done

Environment

Webclient

Windows XP

Windows 7

Windows Server 2003

Windows Server 2008

Cause

If only Cyberstation was installed, but webclient is needed will installing webclient over the top work

Resolution

The recommended installation of webclient when Cyberstation has been installed first is as follows:

Uninstall of Cyberstation, reboot and then a install webclient. Trying to install over the top will not install the needed web components.

You should run the C:\Windows\Microsoft.NET\Framework\v2.0.50727\aspnet_regiis.exe -i command after the install to re-register .net framework with IIS.

Labels (1)
No ratings