New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Illegal object name characters in StruxureWare Building Operation

Issue

What constraints must be followed when naming objects in StruxureWare Building Operation?

Product Line

EcoStruxure Building Operation

Environment

  • Building Operation Workstation
  • Object naming
  • Illegal characters

Cause

Using incorrect object names can may cause unpredictable results in SmartStruxure.

Resolution

Refer to WebHelp article #6429


All objects in the StruxureWare database have to have a name. StruxureWare is case-sensitive and differentiates between upper and lowercase characters.

Two objects cannot be named in the same way in the same folder even if the objects are of different types. For example, you cannot create an alarm named Building A and a graphic named Building A in the same folder. However, if you name the graphic Building a, with a lowercase a, you can create it in the same folder as the alarm object Building A.

The following characters are not allowed in object names in StruxureWare Building Operation.         

  • /
  • "
  • ?
  • *
  • ~
  • &
  • White space is not allowed in the beginning or the end of an objects name.
  • . (period) is not allowed in the beginning of an objects name.
  • There is no limitation of how many characters an object name can have.

NOTE: If an apostrophe (') is used in the Enterprise Server name, Webstation will have some issues with page links. Page links do not work in Webstation but work in Workstation has more information about this issue.

Tags (9)
Labels (1)
No ratings