Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

ID Works Setup with TAC I/NET 2.4X and Windows 7 64-bit

Issue

How to set up ID Works 6.5 in Windows 7 64-bit.

Product Line

TAC INET

Environment

  • ID Works version 6.5
  • I/Net Seven rev 2.4X
  • SQL2008 R2 (Full)
  • SQL2008 R2 Express

Cause

Normally this is needed for an upgrade or a new install of ID Works and I/Net Seven on a new Windows 7 64-bit PC.

Resolution

See ID Works Win7 64-bit Setup.pdf for step by step instructions for setup.

Tags (3)
Labels (1)
No ratings
Contributors