New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements

- Who are the top users of September? Discover them here!

- Check out the ESS Active Energy Management Blog now! 

- Join us on October 23rd for a live Panel session to discuss The Power of a Sustainable Ecosystem with Hervé Coureil, Chief Digital Officer of Schneider Electric and other great speakers. Register here!

ID Works Limitations when configured with I/NET Seven

Issue

  • What are the limitations of using ID Works with I/NET Seven?
  • Can a "begin time" or an "end time" be assigned to a temporary card from ID Works (Card Access Control Data Entry)?
  • Can an individual’s record be made a "DPU Resident" from ID Works? (I/NET Seven 1.0x)
  • What is the format of the CardID entry in the ID Works system?
  • Can assign PIN numbers be used with an ID Works system?

Product Line

TAC INET

Environment

Cause

I/NET Seven provides support for Datacard ID Works identification software. I/NET Seven provides a database view specifically designed for use with ID Works. This view contains tenant and individual data used by the ID Works Video Badging application. It allows you to add individuals, assign key/cards, edit individual parameters, or even delete individuals. 

The limitations described below are imposed anytime that you use ID Works to modify your I/NET Seven access control system.

Resolution

The limitations described below are imposed anytime that you use ID Works to modify your I/NET Seven access control system.

  1. ID Works does not allow you to add or modify multiple cards for a single individual.
  2. ID Works does not allow you to remove a card from an individual without deleting the individual record in I/NET Seven.
  3. You cannot disable an individual’s card without disabling the individual in the I/NET Seven.
  4. You cannot create a new group or a new tenant from within ID Works.
  5. You cannot assign a begin time or an end time to a temporary card from ID Works – only dates can be entered. I/NET Seven will use a default time of 00:00 (Midnight) on the dates specified. If you need to change this default time, it requires you to go into I/NET Seven > Access > Individuals editor.
  6. You cannot make an individual’s record be DPU resident from ID Works.
  7. You cannot assign a decimal card number to an individual from within ID Works. The format for this entry has to be a hexadecimal number.
  8. You cannot set and individual’s APB scheme (i.e., hard, soft, or graced antipassback) from within ID Works.
  9. You cannot assign a PIN to an individual from within ID Works. These can be access via the I/NET individual editor.

For further information refer to TCON301 Chapter 5.

Tags (3)
Labels (1)
No ratings