Issue
Is it possible to just install the IA Commissioning Tool (WPCT) or IA Flow Balance Tool without having to install WorkPlace Tech?
Product Line
TAC IA Series
Environment
- I/A Series WorkPlace Tech
- I/A Series WorkPlace Tech Commissioning Tool
- I/A Series WorkPlace Tech Flow Balance Tool
Cause
WorkplaceTech is not required on the PC but the operator needs to use the WPCT and or Flow Balancing Tool.
Resolution
It is possible to install the WPCT and/or the IA Flow Balancing software without having to install WorkPlace Tech. At the time of the WorkPlace Tech installation, there are three options to select from:
- WorkPlace Tech Flow Balance Tool
- Workplace Tech Commissioning Tool
- WorkPlace Tech 5.x.
WorkPlace Tech Flow Balancing Tool is preselected. It cannot be deselected – it must be installed. You can choose to install the WorkPlace Commissioning Tool by selecting it. If WorkPlace Tech is not needed then do not select the box next to it. WorkPlace Tech will not be installed during the installation process.