Issue
I have upgraded a BAS site to Sigma, but my controllers will not return correct values when using my Lookosn.rec files.
Environment
Sigma
Cause
Lookosn.rec are not used with Sigma.
Resolution
All controller specific tables must be copied to the universal Lookup.rec. These should be in the range of 1000 to 1999. By the use of 'Download Lookup Tables' from System Diagnostics, a local copy of Lookup.rec is sent to the controller.