Issue
I have a MN500 with a broken display, what can I replace it with?
Environment
MN500
Cause
Replacement part for broken display.
Resolution
You can purchase a MN50-LCD as a direct replacement if that is all that is required.
If the MN500 is also faulty you will need to upgrade to the MN550 which will require Visisat 2.1 Build 137 (as a minimum) to program/convert it.
If the MN500 is on a network then you will need to purchase the MN550-XCOM to enable both comm and LCD to be connected.