New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements

Discover the Exchange Community Top members of August

I/NET Site Inventory and best practices

Issue

Inventory and Serial Numbers for each of the Host Computers

Product Line

TAC INET

Environment

I/NET sites or Multiple I/NET sites under your responsibility

Cause

Desire to be organized and have site information quickly available

Resolution

The easiest way to collect the Serial Number and Version is from Help > About INET.

Request a screen capture of each workstation with I/NET installed. This will give you the exact release, build, User/Site names and the serial number.
Below is the splash screen which is seen when I/NET is opened:

Then organize in a spreadsheet or folder structure which is kept up to date with any changes in the field.

The trick is to have the correct screen capture from the correct computer. Designating as a File Master, Equalized Client, Remote Client, or Stand Alone would also be beneficial to have. Host Number for each Host Computer and a Static IP address would be excellent to keep in the spreadsheet.

Tags (2)
Labels (1)
No ratings