New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements

- Who are the top users of September? Discover them here!

- Check out the ESS Active Energy Management Blog now! 

- Join us on October 23rd for a live Panel session to discuss The Power of a Sustainable Ecosystem with Hervé Coureil, Chief Digital Officer of Schneider Electric and other great speakers. Register here!

How to permanently purge all alarms in Vista and start fresh

Issue

How to permanently purge all alarms in Vista and start fresh.

Product Line

TAC Vista

Environment

Vista Workstation alarm queue

Cause

Sometimes alarms can get stuck in the alarm queue during certain engineering processes. In later versions, these can be erased using the purge feature.

Resolution

  1. To get rid of all old alarms in Vista, browse to the database location:
    C:\Program Files\TAC\TAC Vista 5.x.x\Db\$thisdb
    Note: The example is using the default database path for Vista. If you are unsure of the database location, go to Vista Server Setup where your Vista Database path is from the Vista Database tab.
  2. Shutdown the Vista Server if it is currently running.
  3. In the vista DB folder, rename $this.alr and $this_bp.alr to something else (e.g. this.alr.old) for future offline use, or delete the files permanently.
  4. Restart the Vista server, and the alarms should be cleared with the exception of current active alarms.
Tags (1)
Labels (1)
No ratings