New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

How to configure auxiliary contact on SE7000

Issue

Unable to utilize auxiliary contact on SE7000

Environment

  SE7000

Cause

Misunderstanding of wiring and configuration steps for the auxiliary output

Resolution

SE7600

The Aux contact will provide 24 Vac to end devices such as; exhaust fans, valves, economizers, pumps…The contact will operate in conjunction with occupancy command of the thermostat.

 

 

 

 

SE7200 | SE7300

 

The auxiliary output on terminal BO5 terminal 6 and BO5 terminal 7 is a dry contact that require 24 Vac loop to operate.

The output will operate accordingly to configuration and control end devices.

 

Auxiliary contact function and configuration

PLEASE RATE THIS SOLUTION

Tags (1)
No ratings