Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

How to Upgrade the firmware of the AS

Issue

Upgrade the AS to the latest  firmware 

Product Line

EcoStruxure Building Operation

Environment

Windows 

SmartStruxure

Cause

Need instructions on how to Upgrade AS firmware

Resolution

Upgrading the firmware of the AS

Steps:

  1. At first, make sure you disconnect the USB cable and us the ethernet connection as it is a faster way to upgrade the AS
  2. In the Device Administrator click "Add Network Automation Server"  
  3. Write the ip address you just gave at the first line - OK
  4. You should be able to see something like this:

  5. Click the Upgrade Device(s) button      and this will appear:

  6. Click OK to start the process
  7. After a while, you should get "Install finished successfully!" to the Upgrade status column

Now you can close the StruxureWare Device Administrator

Tags (5)
Labels (1)
100% helpful (1/1)