Issue
How many global objects can be used in a Sigma controller or IC?
Environment
X96 controllers
X32 controllers
Integration controllers - All types
Cause
Configuration and engineering issue.
Resolution
A controller or IC can have a maximum of 50 received globals. There are no such restrictions on the number of globals a controller can transmit, but when engineering a Sigma system, additional communications and loading on the controller must be taken into account.