Issue
How can the Niagarad service for Niagara G3 be started?
Environment
- Niagarad service
- Niagara G3
Cause
There are three different ways to start the Niagarad service manually.
Resolution
- From the Windows Start menu: click Programs > Vykon AX Supervisor 3.x.x > Install Platform Daemon
- Open a DOS window and type - cd\Niagara\Niagara-3.x.x\bin then type plat.exe installdaemon
- Create a desktop shortcut with the following: C:\niagara\niagara-3.x.x\bin\plat.exe installdaemon