Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Help on TGML scripting and advanced features

Issue

Where can I find help on TGML scripting and advanced features? Which javascript functions are supported and how do these impact performance.

Product Line

TAC Vista

Environment

TAC Vista TGML graphics editor 5.1.7

Cause

More advanced graphics often require scripting and the engineer needs to know which functions are supported.

Resolution

In the TGML editor under Help there is a section called TGML Format Specification. Details of scripting methods as well as examples can be found here.

Also check out the JavaScript Essentials - Episode 3 - Value Types Quick-Help video on the Exchange.

Tags (1)
Labels (1)
No ratings
Contributors